Define Constructional Parameter
Constructional parameters contain information about the system that will not change by time. Example: Material of construction, Construction code with information such as manufacturer name and manufactured year.
Perform the following steps to define the constructional parameters.
-
Navigate Parameter tab. Parameter tab is further categorized into five sections, namely Constructional, Operational, Derived, Predicted and Reference.
Constructional page is displayed by default.
-
Click Add Record button. Add Parameter tab lists all the available parameters.
System Template - Constructional
-
Select the constructional parameters needed for this system template by selecting the check box next to them.
You can also search the required parameters using the search box in the top right corner of the window.
-
Click Add. Selected parameters will be displayed in the Constructional Parameters page.